Have You Tried Ruckus Unleashed Mobile App Yet?
Mobile device management for your Wi-Fi network right from your phone using the mobile app Ruckus Unleashed. Check internet connectivity and do ping tests.
It’s summertime, and the livin’ is easy. And it just got even easier with the Ruckus Unleashed Mobile App, which is all about simplicity and ease of use. Best of all, you now have the option to stay on top of Wi-Fi tasks no matter where you are, so nothing slips through the cracks. Whether you’re at a meeting or at the beach, you can set up Wi-Fi or reconfigure an access point (AP) in a flash. With the Ruckus Unleashed Mobile App, you can do a typical installation or an advanced installation (gateway mode) – and you can even upgrade your Ruckus Unleashed network with simple touch of a button.
The app enables you to take care of common management tasks as well. There’s so much you can do – like run the built-in SpeedFlex capability to test the speed of your Wi-Fi, discover the top applications that are in use on your network, change AP names, create a WLAN, block a client that’s behaving badly, reboot an AP, and much more.
Ruckus Unleashed Mobile App also provides you with some really useful information, complete with graphs and charts. For example, you can see how much traffic has been flowing through a specific AP for the past hour or the past 24 hours. Is that traffic related to the uplink or downlink from the AP perspective? The app can provide this type of WLAN-level information too. If Internet connectivity is down, you’ll see that right on the dashboard. Then you can do some basic troubleshooting using ping test or trace route.
The Ruckus Unleashed Mobile App helps you hit the air running. You can do your job better and keep users and your manager smiling as you keep the corporate Wi-Fi humming.
On the right are some screen shots to give you an idea of our user-friendly graphical interface.
If you haven’t tried it yet, why not give it a shot? Hit the air running with the Ruckus Unleashed Mobile App. It’s available for both Apple iOS and Google Android platforms. Download it today at Google Play and the Apple Store.